Technical FAQs

Ask a Question

Which USB cable is used to connect a Zelio SR3xx to a computer already equipped with Zelio Soft 2?

The part number of the cable required to connect a PC running ZelioSoft2 programming software (SR2SFT02) to the USB communication port on an SR2xx or SR3xx programmable relay is SR2USB01.

The communication lead SR2USB01 has a USB connector on one end and a dedicated Zelio connector on the other, cable length is 3 m.

Was this helpful?
What can we do to improve the information ?