Technical FAQs

Ask a Question

How can I change language on the LTMCU operator control unit?

The LTMCU unit is a pocket operator control unit which can be used to configure LTMR motor management controllers from the TeSys T range.

The LTMCU unit allows the user to choose from several languages stored in an integrated dictionary.
English has been integrated in this product by default.

The LTMCU LangTool software can be used to download and install 2 languages on the LTMCU unit. 
This is free software, to access the relevant software downloads Serach for "LTMCU". 
On the page presented , the two software files to download are: LTMCU Langtool Software and LTMCU_languages.
Was this helpful?
What can we do to improve the information ?