Technical FAQs

Ask a Question

Should the metal parts of the XB4 range be earthed?

If an XB4 button has to be installed on an insulating support, the metal parts of this button must always be earthed.

There are no earthing plates specific to the XB4 range.

The best way around the problem of mounting a button on an insulating support is to use the XB5 plastic range.

Was this helpful?
What can we do to improve the information ?