Technical FAQs

Ask a Question

What is the accuracy class of ME type electronic kilowatt-hour meters.

The accuracy class = 1

The error on the measurement is less than 1%. The test conditions are: for 230 VAC at 50 Hz, for currents between 3 and 65 A, and for a cos Phi of 0.5.
Was this helpful?
What can we do to improve the information ?