Technical FAQs

Ask a Question

Which programming software replaces TwidoSoft?

The TwidoSoft software has been replaced by the TwidoSuite programming software,  part number (on DVD-ROM) is: TWDBTFU10M
The transfer cable or Bluetooth adaptor must be ordered separately. The transfer cables are: TSXPCX1031 for connection to the PC's serial port. TSXCUSB485 converter in conjunction with the TSXCRJMD25 cable for connection to the PC's USB port.
Note:  The following TwidoSoft CD-ROM packs are no longer sold: TWDSPU1002V10M - CD-ROM only, TWDSPU1001V10M - CD ROM with TSXPCX1031 cable, TWDSPU1003V10M - CD ROM with TSXPCX3030 cable, TWDSPU1004V10M - CD-ROM with VW3A81114 Bluetooth adaptor.
Was this helpful?
What can we do to improve the information ?