Technical FAQs

Ask a Question

What is the maximum distance between a light sensitive switch and its photoelectric cell?

The maximum distance between a light-sensitive switch and its photoelectric cell is:
100 m with 1.5 mm² cable
60 m max. with 0.75mm² cable

Caution:
Do not run the light sensitive switch to photoelectric cell connecting cables with the 220 V power conductors.
Was this helpful?
What can we do to improve the information ?