Technical FAQs

Ask a Question

How can I find a lost code on Sepam 2000?

To find the lost code on a Sepam 2000 prior to 96/49:

go to the control logic in which the code (password) is given
 
To find the lost code of a Sepam 2000 later than or equal to 96/49, there are 2 options:

If the code has not been modified using the Pocket PC:
  • go to the control logic in which the code (password) is given.
If the code has been modified using the Pocket PC: 
  • re-load the control logic using LOGIPAM making a note of the code (password) used.

Note: The standard code (password) for the control logics is 6543210.
Was this helpful?
What can we do to improve the information ?