Technical FAQs

Ask a Question

What is the Degree of Protection (IP) of an external protection enclosure for a TRIHAL transformer?

For indoors, the standard protection enclosure of the TRIHAL transformer is IP 31. For non-standard and indoors, an IP 23 enclosure for a polluted atmosphere can be installed. For outdoors and customised transformers, an IP 35 minimum protection enclosure can be ordered.
Was this helpful?
What can we do to improve the information ?