Technical FAQs

Ask a Question

How do I connect a potentiometer on an RE7CV time delay relay?

When using RE7CV relays with time delay adjustment potentiometers, the potentiometers must be connected in the following way:

To set the time in off-delay mode  the opposite ends of the potentiometer must be connected to  Z1 and Z2.
The potentiometer wiper is connected to Z2. See (7) below

To set the time in on-delay  mode the opposite ends of  the potentiometer must be connected to Z2 and Z3.
The potentiometer wiper is  connected to Z2. See (8) below.

The potentiometer should be 47K Ohm Linear Type, rated at 0.2W or greater, which are not sold by Schneider.

Was this helpful?
What can we do to improve the information ?