Technical FAQs

Ask a Question

What are the dimensions of the metal guards, part number ZBZ1600, for the emergency stop function?

The dimensions of the metal guards for the XB4 and XB5 ranges of diameter 22 emergency stop pushbuttons are as follows:
Was this helpful?
What can we do to improve the information ?