Technical FAQs

Ask a Question

What part number replaces the TSXPCX3030 programming cable?


The PLC programming cable via PC USB port, part number TSXPCX3030, is replaced by TSXCUSB485. This is a multifunction programming cable which can be used for multiple types of hardware connection and configuration, consequently the use of a second cable (link cable) is required; please consult the diagram below:




  
Was this helpful?
What can we do to improve the information ?