Technical FAQs

Ask a Question

Can I divide the XPEMxxD double foot switches into 2 XPEMxx single foot switches?

All double foot switch part numbers can be made up using the part numbers for single foot switches, combining them with a protective guard.

They consist of the part number for foot switches without a protective guard.

Caution: You must use the part numbers associated with a specific device (trigger mechanism or not), but also of the same colour.

For example we can break down the part number XPEM6210D, which corresponds to the combination of

part number XPEM211 (2 steps - 2 "N/C + N/O") on the left and
part number XPEM110 (1 step - 1 "N/C + N/O") on the right.

These 2 foot switches are protected against unintended operation by a double metal protective guard, part number XPEZ9xx.

  • XPEZ921 corresponds to a blue double protective guard for an XPEM metal foot switch


  • XPEZ931 corresponds to an orange double protective guard for an XPER metal foot switch

 (Product data sheet Attached)

Was this helpful?
What can we do to improve the information ?