Technical FAQs

Ask a Question

What are the part numbers of the metal boxes with tapped cable inlets for M20x1.5 cable glands?

For virtually all XAPMxx box models we offer an H29 version, which is tapped at 20 x 1.5 intervals (6 to 12 mm diameter).
The cable gland is a vibration-damping mechanical clamp with neoprene seal.
The locking section consists of flexible strips which exert strong pressure on the cable, making the product exceptionally robust.
Was this helpful?
What can we do to improve the information ?