Technical FAQs

Ask a Question

How can I find the IP address of an already configured TSXETZ510 module?

Like any Schneider Electric product with an Ethernet port, the TSXETZ510 module is configured with a default IP address.

This IP address can be modified via the Web pages predefined in the module.

Once it has been reconfigured, the default IP address will no longer work and you cannot restore the factory settings.

However, on the TSXETZ510 module, which has an RS232 serial port, you can find the configured IP address by following the steps in section 3.4 of the attached guide.


 
Was this helpful?
What can we do to improve the information ?