Technical FAQs

Ask a Question

What is the maximum number of units that can be assembled on an XVP beacon tower?

It is possible to stack a combination of up to 5 illuminated and audible units (one audible unit maximum) to create an XVP beacon tower. 

Example 1: 5 illuminated lens units 
Example 2: 4 illuminated lens units + 1 audible signaling unit
Was this helpful?
What can we do to improve the information ?