Technical FAQs

Ask a Question

How many sensors can I place on the temperature inputs T1 and T2 of a LTMR motor management controller?

The motor temperature is monitored via an LTMR motor management controller using PTC (or NTC) sensors installed on the motor coils.

The motors generally have a total of 3 sensors (one per motor coil), but it is possible for the motor have fewer sensors. 

The maximum resistance threshold permitted by the module between T1 and T2 is 6500 ohms.

This value corresponds to that of 3 PTC (or NTC) sensors connected in series and wired on the T1 and T2 inputs of the module.


Was this helpful?
What can we do to improve the information ?