Technical FAQs

Ask a Question

What is the radius of curvature of an ASI cable?

The TPE ASi cable, XZCBxxxxxH, has been tested for flexible mounting: 300,000 operations.
 It is preferable to use the TPE version, part number XZCBxxxH, as the radius of curvature behavior with regard to the thickness is better than the standard cable.

Possible use of the standard or the TPE ASi cable depends on the characteristics of these two cables: class 6.
For the standard cable, the radius of curvature of the XZCB flat rubber cable is:
  • 15 mm across the thinnest section
  • 0 mm across the thickest section.

The radius of curvature of the XZCB TPE cable is:
  • 20 mm across the thinnest section
  • 60 mm across the thickest section.

Was this helpful?
What can we do to improve the information ?