Technical FAQs

Ask a Question

What is the specific inrush current on the output contacts of the LTMR controller?

The maximum load current permitted on the output contacts is 5 A at 250 VAC or 30 VDC
Was this helpful?
What can we do to improve the information ?