Technical FAQs

Ask a Question

What Size are the fixing screws supplied with the Ultimate Flat plate range of accessories?

Provided with each of the accessories are two sets of fixing screws, set one measures M3.5 x 25mm and the second set measures M3.5 x 30mm.
Was this helpful?
What can we do to improve the information ?