Technical FAQs

Ask a Question

What is the maximum split configuration on the new 12 way flexible split load Easy9+ Consumer unit EZ9EFS12CU ?

The maximum split configuration on the 12 way flexible split load Easy9+ consumer unit has a Max of 4 unprotected, Max of 7 on RCD 1 and a Max of 7 on RCD 2. The values given highlight maximum ALLOWABLE ways only, the installer will only be able to achieve up to 12 outgoing ways with this product.
Was this helpful?
What can we do to improve the information ?