Technical FAQs

Ask a Question

I have sent a TwidoSuite project to someone but they can't open it, how should I save the project so that they can open it?

To send a TwidoSuite project via email etc, it should be saved as an archive file.
  1. Select the 'Project' tab
  2. Select 'Save current project'
  3. Select the file format as 'TwidoSuite archive', then save.
The project is then saved as a single archive file (.xar).  By default, it will be saved under C:\Program Files\Schneider Electric\TwidoSuite\My Projects.




 
Was this helpful?
What can we do to improve the information ?