Technical FAQs

Ask a Question

When putting a Zelio Logic relay into Run mode, what does ‘WITH NONVOLAT INI’ and ‘NO NONVOLAT INI’ mean?

When putting a Zelio Logic relay in to ‘Run’ mode, there are three options;
1.       WITH NONVOLAT INI
All current values in counters, timers etc are reset to zero before the relay starts.
 
2.       NO NONVOLAT INI
The current values will be retained on start up for any counters, timers etc that have been configured with the ‘latching’ option.
 
3.       NO
The program will not be started.
 



Use the UP and DOWN arrow button to select, the active selection flashes on and off, confirm with Menu/Ok button.
Was this helpful?
What can we do to improve the information ?