Technical FAQs

Ask a Question

We want the facility to remove the handheld HMI from junction box ref XBTGH2460. Is there an adaptor to take its place so that the emergency stop circuit is not activated?

Reference XBTZGHCAP is an adaptor that plugs into the XBTGH2460 junction box which shunts the emergency stop circuit allowing the handheld HMI to be disconnected.
 It is a "loopback plug" for the safety circuit allowing the safety circuit to be enabled with out the XBTGH2460 in circuit.
Note: Extreme caution should be applied because the Safety System has been altered by the removal of this device, a Risk Assessment should be carried out to ensure safety compliance.
Was this helpful?
What can we do to improve the information ?