Technical FAQs

Ask a Question

What is the minimum and maximum thickness of wall our dry lining boxes (GDL1 & GDL2) can be installed in?

The minimum thickness is 2 mm and the maximum thickness is up to 17 mm.
Was this helpful?
What can we do to improve the information ?