Technical FAQs

Ask a Question

Are the KQ MCBS compatible with the new SE type distribution boards?

Yes the KQ mcbs are compatible with SE type boards, as are the SE mcbs are backward compatible with the KQ range.
Was this helpful?
What can we do to improve the information ?