Technical FAQs

Ask a Question

Which Quadbreak cable box do I require?

The following chart provides the product code of the recommended cable box for each rating of Quadbreak fuse switch disconnector

 
63A SQBX100
100A
160A SQBX160
200A SQBX250
250A
315A SQBX500
400A
500A
630A SQBX630
800A
Was this helpful?
What can we do to improve the information ?