Technical FAQs

Ask a Question

What is the maximum weight a circular dry lining box can support?

Our circular dry lining box (product code CRB2W) will support a maximum of 3 kg at a temperature of 60 degrees C
Was this helpful?
What can we do to improve the information ?