Technical FAQs

Ask a Question

What range of Finishes are available in the KNX ARGUS Presence detectors ?

The KNX ARGUS Presence detectors are available in a  Polar white and Aluminum finish including the KNX ARGUS 220 product.The KNX ARGUS Presence 180/2.20 flush mounted is also available in a Anthracite,Glossy Polar white and a Aluminum finishes. 
Was this helpful?
What can we do to improve the information ?