Technical FAQs

Ask a Question

Is there a surface mounted option available for the KNX ARGUS Presence detectors?

The surface mounted housing for the KNX ARGUS Presence device is available to order.Product code MTN550619 in a Polar white finish.The housing will only accept the following Detectors,ARGUS Presence MTN550590, ARGUS Presence with IR receiver and for extension unit operation MTN550591,ARGUS Presence Basic MTN6307.. ,KNX ARGUS Presence MTN6308.. and the KNX ARGUS Presence with light control and IR receiver MTN6309..
Was this helpful?
What can we do to improve the information ?