Technical FAQs

Ask a Question

What would be the Range and the Angle of detection for the KNX Argus Presence detector ?

The Angle of detection is 360 degrees with a Range of a maximum 7 metres at a mounting height of 2.50 metres.
Was this helpful?
What can we do to improve the information ?