Technical FAQs

Ask a Question

What would be the Range and the Angle of detection for the KNX Argus Presence Basic detector?

The KNX Presence Basic Detector has a maximum range of 7 metres throughout the Angle of Detection radius of 360 degree at a mounting height of 2.50 metres.
Was this helpful?
What can we do to improve the information ?