Technical FAQs

Ask a Question

What is the Detection Range and the Angle of Detection of the KNX Argus 180 flush mounted movement detector?

The detection range of the KNX Argus 180 flush mounted detector  is 8 metres at a mounting height of 1.1 metres.The  Angle of detection is 180 degree.
Was this helpful?
What can we do to improve the information ?