Technical FAQs

Ask a Question

What is the Range and the Angle of Detection of the KNX Argus 220 movement detector?

The maximum range is 16 metres,with a Angle of Detection of 220 degree.This particular detector has a 360 degree short range zone of approx 4 metres.
It is also possible to to blank out individual lens areas.
Was this helpful?
What can we do to improve the information ?