Technical FAQs

Ask a Question

Can I source extra socket mounting boxes for the Power Pole/Power Post if required?

Yes, for the PP18 &  PS1865W  the product code is CLB314W (25mm deep), for the PP28/PS2863/PP38W the product code is PPBA11W (25mm deep) and for use with the PP38W only a 35 mm deep version is available  the product code is PPBA21W.
Was this helpful?
What can we do to improve the information ?