Technical FAQs

Ask a Question

Will the Powerline Sockets work on 60Hz carrier (most ships use this)?

Yes, the Powerline Sockets works perfectly well in the US on 60 Hz. The timing hertz range does not matter as long as it is a constant. If it cannot be constant an internal clock on the Powerline chip will be used.
Was this helpful?
What can we do to improve the information ?