Technical FAQs

Ask a Question

What is the range of the Connect Radio System wireless controllers?

The direct point to point range between 2 devices inside a building is approximately 30 meters but this may be reduced by obstructions (walls, floors etc.). The Connect Radio System uses a mesh technology however, so it is possible for the signal to be routed through 3 additional mains powered devices before reaching its intended target, depending upon the location of the devices this could increase the range of operation well beyond what would be possible with a direct point to point type RF device.
Was this helpful?
What can we do to improve the information ?