Technical FAQs

Ask a Question

Do I need to measure the quality of the wiring?

 In general, the wiring quality is not measured before a Powerline installation.  The most important factor is the amount of electrical noise the building wiring is subject to.  Our tests have shown excellent results in a house with old wiring because it had relatively few electrical devices whereas performance was initially lower in a modern house with numerous dimmers and transformers.  Where ever possible, it helps to plug the noisy devices into the filtered socket on the front of the product to isolate the noise makers from power ring.
Was this helpful?
What can we do to improve the information ?