Technical FAQs

Ask a Question

What is the limit in terms of total number of units and the available bandwidth?

The total number of Powerline Sockets within a single network is 64 units with the bandwidth divided amongst units (i.e. one collision domain like a hub).

 

The bandwidth is shared amongst all the units and is currently 200Mbps (gross).

Was this helpful?
What can we do to improve the information ?