Technical FAQs

Ask a Question

Can I replace the backlight in an XBTGT HMI?

It is possible for a customer to replace the backlight in certain HMIs, but not all of them.

The XBTGT5000/6000 and 7000 series HMI backlights can be replaced by the customer, the attached file shows the part references for the appropriate backlights.

The XBTGT1000/2000 and 4000 HMIs backlights cannot replaced by the customer.  If the backlights need replacing, please contact your local distributor.
Was this helpful?
What can we do to improve the information ?