Technical FAQs

Ask a Question

What size extension collars are available for use with dado trunking?

Extension collars are compatible for use with Ultimate 60, Ultimate 62, Cableline 50 & Cableline 40 ranges of dado trunking and are available in the following sizes:

1 gang 10mm deep     CEC110W
1 gang 19mm deep     CEC119W
2 gang 10mm deep     CEC210W
2 gang 19mm deep     CEC219W

Extension collars can be used to mount wiring accessories where additional depth is required.
Was this helpful?
What can we do to improve the information ?