Technical FAQs

Ask a Question

What size padlock can i use on the NSX MCCB lock off device 29370?

The NSX MCCB lock off 29370 padlocking system will accept up to three  padlocks with shackle diameters ranging from 5 to 8 mm. Compatible with the NSX, MGP CDXAE, CNXAE CHXAE range of MCCB's.
Was this helpful?
What can we do to improve the information ?