Technical FAQs

Ask a Question

What is the default IP address of a TSXETG30** FactoryCast HMI Gateway Module?

The default IP address for a TSXETG30** module is 10.10.xx.xx, the last two octets being derived from the last two octets of the MAC address.  The last two octets need to be converted from hexadecimal to decimal

For example, if the MAC address is 00.80.F4.03.81.34, the hex values 81 and 34, convert to 129 and 52 in decimal. 

The default IP address would therefore be
Was this helpful?
What can we do to improve the information ?