Technical FAQs

Ask a Question

What Schneider Electric Drive has replaced the Telemecanique Altivar ATV68

There are two possible replacements as the ATV68 could be used on High Torque applications or on Standard Torque applications so listed below are the possible replacements

Three Phase Supply 400.....500V 50/60H

High Torque Applications (150% Tn)

ATV68C10N4 ATV71HD75N4

ATV68C13N4 ATV71HD90N4

ATV68C15N4 ATV71HC11N4

ATV68C19N4 ATV71HC13N4

ATV68C23N4 ATV71HC16N4

ATV68C28N4 ATV71HC20N4

ATV68C33N4 ATV71HC25N4

ATV68C43N4 ATV71HC31N4

ATV68C53N4 ATV71HC40N4

ATV68C63N4 ATV71HC50N4


ATV68FC10N4 ATV71HD75N4 With Encoder card 

ATV68FC13N4 ATV71HD90N4 With Encoder card 

ATV68FC15N4 ATV71HC11N4 With Encoder card 

ATV68FC19N4 ATV71HC13N4 With Encoder card 

ATV68FC23N4 ATV71HC16N4 With Encoder card 

ATV68FC28N4 ATV71HC20N4 With Encoder card 

ATV68FC33N4 ATV71HC25N4 With Encoder card 

ATV68FC43N4 ATV71HC31N4 With Encoder card 

ATV68FC53N4 ATV71HC40N4 With Encoder card 

ATV68FC63N4 ATV71HC50N4 With Encoder card 


Standard Torque Applications (120% Tn)

ATV68C10N4 ATV61HD90N4

ATV68C13N4 ATV61HC11N4

ATV68C15N4 ATV61HC13N4

ATV68C19N4 ATV61HC16N4

ATV68C23N4 ATV61HC20N4

ATV68C28N4 ATV61HC25N4

ATV68C33N4 ATV61HC31N4

ATV68C43N4 ATV61HC40N4

ATV68C53N4 ATV61HC50N4

ATV68C63N4 ATV61HC63N4


ATV68FC10N4 ATV71HD75N4 With Encoder card 

ATV68FC13N4 ATV71HD90N4 With Encoder card 

ATV68FC15N4 ATV71HC11N4 With Encoder card 

ATV68FC19N4 ATV71HC13N4 With Encoder card 

ATV68FC23N4 ATV71HC16N4 With Encoder card 

ATV68FC28N4 ATV71HC20N4 With Encoder card 

ATV68FC33N4 ATV71HC25N4 With Encoder card 

ATV68FC43N4 ATV71HC31N4 With Encoder card 

ATV68FC53N4 ATV71HC40N4 With Encoder card 

ATV68FC63N4 ATV71HC50N4 With Encoder card

 

Was this helpful?
What can we do to improve the information ?