Technical FAQs

Ask a Question

What are the maximum permitted loads in Watts for multiple electronic dimmer modules in a single enclosure?

Front plate gang size 2 3 4 6 8 9 12 18 24
Per row (max rating W) 400 480 480 480 480 480 480 480 480
Total plate (max rating W) 400 480 480 740 740 940 940 1440 1800
Was this helpful?
What can we do to improve the information ?