Technical FAQs

Ask a Question

What Schneider Electric Drive has replaced the Telemecanique Altivar ATV66

There are two possibilities due to the fact the ATV66 could be used as a Constant Torque or a Variable Torque drive. So the application the drive is being used in would be of great advantage. The replacements have been separated into Constant and Variable Torque groups

The list below gives the nearest alternative(s) :Constant Torque Applications

Three Phase Supply 200...240V 50/60Hz

ATV66U41M2 ATV71H075M3

ATV66U41M2 ATV71HU15M3

ATV66U41M2 ATV71HU22M3

ATV66U72M2 ATV71HU30M3

ATV66U90M2 ATV71HU40M3

ATV66D12M2 ATV71HU55M3

ATV66D16M2 ATV71HU75M3

ATV66D23M2 ATV71HD11M3X

ATV66D33M2 ATV71HD22M3X

ATV66D46M2 ATV71HD30M3X

Three Phase Supply 400.....500V 50/60H

ATV66U41M2 ATV71H075N4

ATV66U41M2 ATV71HU15N4

ATV66U41M2 ATV71HU22N4

There are two possibilities due to the fact the ATV66 could be used as a Constant Torque or a Variable Torque drive. So the application the drive is being used in would be of great advantage. The replacements have been separated into Constant and Variable Torque groups

The list below gives the nearest alternative(s) :Constant Torque Applications

Three Phase Supply 200...240V 50/60Hz

ATV66U41M2 ATV71H075M3

ATV66U41M2 ATV71HU15M3

ATV66U41M2 ATV71HU22M3

ATV66U72M2 ATV71HU30M3

ATV66U90M2 ATV71HU40M3

ATV66D12M2 ATV71HU55M3

ATV66D16M2 ATV71HU75M3

ATV66D23M2 ATV71HD11M3X

ATV66D33M2 ATV71HD22M3X

ATV66D46M2 ATV71HD30M3X

Three Phase Supply 400.....500V 50/60H

ATV66U41M2 ATV71H075N4

ATV66U41M2 ATV71HU15N4

ATV66U41M2 ATV71HU22N4

ATV66U54N4 ATV71HU30N4

ATV66U72N4 ATV71HU40N4

ATV66U90N4 ATV71HU55N4

ATV66D12N4 ATV71HU75N4

ATV66D16N4 ATV71HD11N4

ATV66D23N4 ATV71HD15N4

ATV66D33N4 ATV71HD22N4

ATV66D46N4 ATV71HD30N4

 

ATV66D54N4 ATV71HD37N4

ATV66D64N4 ATV71HD45N4

ATV66D79N4 ATV71HD55N4

ATV66C10N4 ATV71HD75N4

ATV66C13N4 ATV71HD90N4

ATV66C15N4 ATV71HC11N4

ATV66C19N4 ATV71HC13N4

ATV66C23N4 ATV71HC16N4

ATV66C28N4 ATV71HC20N4

ATV66C31N4 ATV71HC25N4

VariableTorque Applications

Three Phase Supply 200...240V 50/60Hz

ATV66U41M2 ATV61H075M3

ATV66U41M2 ATV61HU15M3

ATV66U41M2 ATV61HU22M3

ATV66U72M2 ATV61HU30M3

ATV66U90M2 ATV61HU40M3

ATV66D12M2 ATV61HU55M3

ATV66D16M2 ATV61HU75M3

ATV66D23M2 ATV61HD11M3X

ATV66D33M2 ATV61HD22M3X

ATV66D46M2 ATV61HD30M3X

Three Phase Supply 400.....500V 50/60H

ATV66U41M2 ATV61H075N4

ATV66U41M2 ATV61HU15N4

ATV66U41M2 ATV61HU22N4

ATV66U41N4 ATV61HU30N4

ATV66U54N4 ATV61HU40N4

ATV66U72N4 ATV61HU55N4

ATV66U90N4 ATV61HU75N4

ATV66D12N4 ATV61HD11N4

ATV66D16N4 ATV61HD15N4

ATV66D23N4 ATV61HD18N4

ATV66D33N4 ATV61HD22N4

 

ATV66D33N4 ATV61HD30N4

ATV66D46N4 ATV61HD37N4

ATV66D54N4 ATV61HD45N4

ATV66C64N4 ATV61HD55N4

ATV66D79N4 ATV61HD75N4

ATV66C10N4 ATV61HD90N4

ATV66C13N4 ATV61HC13N4

ATV66C15N4 ATV61HC16N4

ATV66C23N4 ATV61HC20N4

ATV66C23N4 ATV61HC25N4

ATV66C31N4 ATV61HC25N4


Low Noise VariableTorque Applications

Three Phase Supply 200...240V 50/60Hz

ATV66U41M2 ATV61H075M3

ATV66U41M2 ATV61HU15M3

ATV66U41M2 ATV61HU22M3

ATV66U72M2 ATV61HU30M3

ATV66U90M2 ATV61HU40M3

ATV66D12M2 ATV61HU55M3

ATV66D16M2 ATV61HU75M3

ATV66D23M2 ATV61HD11M3X

ATV66D33M2 ATV61HD22M3X

ATV66D46M2 ATV61HD30M3X

Three Phase Supply 400.....500V 50/60H

ATV66U41M2 ATV61H075N4

ATV66U41M2 ATV61HU15N4

ATV66U41M2 ATV61HU22N4

ATV66U54N4 ATV61HU30N4

ATV66U72N4 ATV61HU40N4

ATV66U90N4 ATV61HU55N4

ATV66D12N4 ATV61HU75N4

ATV66D16N4 ATV61HD11N4

ATV66D23N4 ATV61HD15N4

ATV66D33N4 ATV61HD22N4

ATV66D46N4 ATV61HD30N4

ATV66D54N4 ATV61HD37N4

ATV66D64N4 ATV61HD45N4

ATV66D79N4 ATV61HD55N4

 

ATV66U54N4 ATV71HU30N4

ATV66U72N4 ATV71HU40N4

ATV66U90N4 ATV71HU55N4

ATV66D12N4 ATV71HU75N4

ATV66D16N4 ATV71HD11N4

ATV66D23N4 ATV71HD15N4

ATV66D33N4 ATV71HD22N4

ATV66D46N4 ATV71HD30N4

 

ATV66D54N4 ATV71HD37N4

ATV66D64N4 ATV71HD45N4

ATV66D79N4 ATV71HD55N4

ATV66C10N4 ATV71HD75N4

ATV66C13N4 ATV71HD90N4

ATV66C15N4 ATV71HC11N4

ATV66C19N4 ATV71HC13N4

ATV66C23N4 ATV71HC16N4

ATV66C28N4 ATV71HC20N4

ATV66C31N4 ATV71HC25N4

VariableTorque Applications

Three Phase Supply 200...240V 50/60Hz

ATV66U41M2 ATV61H075M3

ATV66U41M2 ATV61HU15M3

ATV66U41M2 ATV61HU22M3

ATV66U72M2 ATV61HU30M3

ATV66U90M2 ATV61HU40M3

ATV66D12M2 ATV61HU55M3

ATV66D16M2 ATV61HU75M3

ATV66D23M2 ATV61HD11M3X

ATV66D33M2 ATV61HD22M3X

ATV66D46M2 ATV61HD30M3X

Three Phase Supply 400.....500V 50/60H

ATV66U41M2 ATV61H075N4

ATV66U41M2 ATV61HU15N4

ATV66U41M2 ATV61HU22N4

ATV66U41N4 ATV61HU30N4

ATV66U54N4 ATV61HU40N4

ATV66U72N4 ATV61HU55N4

ATV66U90N4 ATV61HU75N4

ATV66D12N4 ATV61HD11N4

ATV66D16N4 ATV61HD15N4

ATV66D23N4 ATV61HD18N4

ATV66D33N4 ATV61HD22N4

 

ATV66D33N4 ATV61HD30N4

ATV66D46N4 ATV61HD37N4

ATV66D54N4 ATV61HD45N4

ATV66C64N4 ATV61HD55N4

ATV66D79N4 ATV61HD75N4

ATV66C10N4 ATV61HD90N4

ATV66C13N4 ATV61HC13N4

ATV66C15N4 ATV61HC16N4

ATV66C23N4 ATV61HC20N4

ATV66C23N4 ATV61HC25N4

ATV66C31N4 ATV61HC25N4

Low Noise VariableTorque Applications

Three Phase Supply 200...240V 50/60Hz

ATV66U41M2 ATV61H075M3

ATV66U41M2 ATV61HU15M3

ATV66U41M2 ATV61HU22M3

ATV66U72M2 ATV61HU30M3

ATV66U90M2 ATV61HU40M3

ATV66D12M2 ATV61HU55M3

ATV66D16M2 ATV61HU75M3

ATV66D23M2 ATV61HD11M3X

ATV66D33M2 ATV61HD22M3X

ATV66D46M2 ATV61HD30M3X

Three Phase Supply 400.....500V 50/60H

ATV66U41M2 ATV61H075N4

ATV66U41M2 ATV61HU15N4

ATV66U41M2 ATV61HU22N4

ATV66U54N4 ATV61HU30N4

ATV66U72N4 ATV61HU40N4

ATV66U90N4 ATV61HU55N4

ATV66D12N4 ATV61HU75N4

ATV66D16N4 ATV61HD11N4

ATV66D23N4 ATV61HD15N4

ATV66D33N4 ATV61HD22N4

ATV66D46N4 ATV61HD30N4

ATV66D54N4 ATV61HD37N4

ATV66D64N4 ATV61HD45N4

ATV66D79N4 ATV61HD55N4

Was this helpful?
What can we do to improve the information ?