Technical FAQs

Ask a Question

What type of replacement fuse links can be used in Twinbreak switch fuse?

Twinbreak Fuse Links      
Rating BS88 Reference Bussman Reference* GEC Reference
20A A1 44.5mm NITD20 NIT20
32A A2 73mm AA032 TIA32
63A A3 73mm BAO63 TIS63
100A A4 93.7mm CEO100 TCP100
* To conform with ASTA certification Bussman fuses should be used.  
Was this helpful?
What can we do to improve the information ?