Technical FAQs

Ask a Question

What are the MTBF values for the ABL4 range?

These figures are the same for all references in the ABL4 range

MTBF according to standard SN29500 is >500000 hours
MTBF according to MIL Std HDBK217F  is >150000 hours

(Vantive Ref: 1492385)
Was this helpful?
What can we do to improve the information ?