Technical FAQs

Ask a Question

Will the KQ mcb's and rcbo's still trip if there padlock in the on position using the QOEPLA?

Yes, all of the miniature circuit breakers have a "trip free" mechanism which enables them to trip under fault conditions even if the handle is locked ON or held ON manually.
Was this helpful?
What can we do to improve the information ?