Technical FAQs

Ask a Question

When installing 'CLB' boxes in dado trunking, what torque setting should be used?

Using brass inserts 3.2mm upto and including 3.6mm, the torque setting is 0.8Nm (+/-0.08Nm) based on Standard BS4662:2006.

Was this helpful?
What can we do to improve the information ?