Technical FAQs

Ask a Question

What is the IP rating of Shaver sockets?

Our 115/230V dual voltage Ultimate shaver sockets are rated IP41 and are manufactured to BS EN 61558-2-5.
Was this helpful?
What can we do to improve the information ?